Dear all,
To design the power supply of the VCC2, I'm looking for the worst case consumption of the ISO1500. I think this will append when the output is short-circuited. In the datasheet, it is mentionned that IOS= +/-175mA. Following the figure 28, this is the output current measured at the output of the driver. I cannot find the maximum current on ICC2 during that specific case. Is it maximum current (ICC2 driver enabled bus loaded = 80mA) + IOS current (175mA) = 255mA ? If this is not do you have this information ?
Best regards
Arnaud