This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7763: ISO7763FDWR and ISO6763FDWR

Part Number: ISO7763
Other Parts Discussed in Thread: ISO6763,

Dear sir,

A quick question of ISO7763FDWR and ISO6763FDWR:

Customer want to use the pull-up  4.7k ohm resistors  on Pin 7/ Pin 10 of ISO7763FDWR and ISO6763FDWR,  any risk for this?

Background:  customer want to do the 2nd source compatible design in new project,  which is the Enable Pin of  the main source now.

Nice day!

Regards,

Jack