This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO3080: Maximum repetitive RMS isolation voltage/ surge voltage

Part Number: ISO3080
Other Parts Discussed in Thread: ISO1412,

Hello team,

my customer would like to know the RMS value of max repetitive isolation voltage. And they also need surge voltage result under  1.2/50us voltage surge test. Thanks!

  • Hi Zach,

    Thank you for posting to E2E! The RMS value for repetitive isolation voltage of ISO3080 is ~395V, and it does not have a specified surge isolation voltage rating. Since ISO3080 is an older device, please strongly recommend ISO1412 to our customer: it is a newer isolated RS-485 device that is pin-to-pin compatible with ISO3080, is certified to more relevant isolation standards, and is available in Basic and Reinforced isolation options. Below are some of its isolation ratings:



    Please let us know if there are any additional questions.


    Thank you,
    Manuel Chavez

  • Hi Manuel,

    Thanks for your convincing reply! I would recommend the new device to our customer.

    One more question, is there any other other difference between ISO1412 and ISO3080 ( if there is a comparison table )?  Then I could better illustrate the upgrade to the customer. ~~~

    Regards,

    Zach

  • Hi Zach,

    Thanks for considering to recommend the newer devices to customer.
    As requested, I am copying below a comparison table comparing ISO14xx family devices with ISO3080. I am also listing out the key advantages of ISO14xx over ISO308x devices in the following image, thanks.


    Regards,
    Koteshwar Rao

  • Hi Koteshwar,

    Thanks for your detailed comparison! This helps a lot.