Other Parts Discussed in Thread: ISO6741
I found the ISO7741. Is it a FFF drop in replacement?
Thanks,
Kyle
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Kyle,
Thank you for posting, and welcome to E2E! ISO7741 is an FFF replacement for ADUM1401ARWZ-RL and so is ISO6741. It looks like ADUM1401ARWZ-RL has a default output state of HIGH, so ensure to use "non-F" suffix devices (like ISO6741 instead of ISO6741F). If default LOW outputs are needed, or if the default state does not matter, then "F" devices may be used.
TI has a cross reference tool online that helps find which TI devices could be used to replace non-TI devices. Below is the link and a screenshot of how it works using ADUM1401ARWZ-RL as an example:
Link: https://bomcross.ti.com/en/
Please feel free to use this tool anytime, and let us know if you have any additional questions!
Have a great weekend,
Manuel Chavez