Hello dear colleagues,
I hope you are doing well!
I am writing with regard to a technical question -on our ISO7762QDBQQ1- from our customer (Eaton).
Can someone tell me what the output state (HIGH/LOW) is like, if the supply voltage fails on the other side?
From the drawing, the customer interprets that if the TX IN supply is 0V, the RX OUT signal is HIGH. This would be important for the customer because one of the RX signals is a LOW active enable signal.
If, in the absence of a supply on the TX side, the RX signal and thus the enable were HIGH, the output side is in a safe state.
Thanks in advance,
Candas