Hi
could you check whether one TI_ISO6741DWR can drive 5pcs 90E36A SPI bus. (except CS)
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
could you check whether one TI_ISO6741DWR can drive 5pcs 90E36A SPI bus. (except CS)
Hi Gareth,
Thanks for reaching out.
ISO6741 can drive multiple input pins provided the overall capacitive load on its output is <100pF. I checked M90E36A electrical specifications in datasheet but I couldn't find input capacitance of pins SCLK and SDI. If [capacitance(SCLK + SDI) * 5] <100pF, then ISO6741 should be able to drive without any issues. Thanks.
Regards,
Koteshwar Rao