Hello,
We are using ISO7761FQDWQ1 digital isolator in our design.
I want to confirm below point:
In the ISO7761FQDWQ1 IC, 5 channel are forward and 1 is reverse, Considering this case:
Vcci/Vcc1 is the input power supply for the five channel and output power supply for remaning one channel
Vcco/Vcc2 is the output power supply for 5 channel and input power supply is for one channel.
So if the Vcco supply is not present (The input supply for the sixth channel) then the output status of sixth channel should be “Default (LOW)” Please confirm on the same.