Hi Team,
My customer is surveying ISO774x and has a question about power rating.
Below table shows that ISO7740 still can handle 200mW power dissipation at Tj=150C, but datasheet also shows the Max. Tj is 150C. So, when Tj=150C any additional power dissipation can trigger device to thermal projection, right? How can I explain it to customer?
Besides, below diagram shows the power limiting is 0mW when ambient temp. is 150C(the Tj is 150C supposedly). These two data are conflict, isn't it?
BR,
SHH