Hello,
are there any differences between the ISOUSB111 and the XISOUSB111?
When will the ISOUSB111 / XISOUSB111 be available in series and quantities of >100?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Michi,
Thank you for reaching out and for your interest in ISOUSB111.
ISOUSB111 is the part number of the device while the prefix 'X' in the XISOUSB111 only indicates that the X-marked devices are pre-production samples that are only meant for evaluation. ISOUSB111 currently is under PREVIEW status, once the device is fully released then the ISOUSB111 production units will be made available for sale. Till then, only the pre-production samples XISOUSB111 will be available for purchase which should be used for device performance evaluation only and not for production.
I hope that helps you with the clarification, thanks.
Regards,
Koteshwar Rao
When will the ISOUSB111 in production and available?
Please with date or in one, two months...
Hi Michi,
I am sorry to let you know that we do not publish product schedules on E2E forum.
Please subscribe for product updates on ISOUSB111 product page so that you get an update once the device is fully released and production units are available for ordering. When the product is fully released, you will also see the product state go from PREVIEW to ACTIVE state. Please see below screenshot of ISOUSB111 product page where the subscribe option and product status are highlighted with red oval shaped marks. Thanks.
Regards,
Koteshwar Rao