Part Number: ISO1212
Other Parts Discussed in Thread: ISO6721, ISO7720, ISO1211
Hi ISO team,
I saw the ISO1212 VIH and VIL Calculation formula is shown in blow from datasheet.
We can see in the Calculation formula, 8.25V and 7.1V is ISO1212 Fixed threshold voltage.
I have a questions about the threshold voltage.
Why does it set 8.25V and 7.1V rather than 4V and 3V?
If it sets 4V and 3V, so Rthr need use bigger value to get the some VIH/VIL, which more power dissipation move to Rthr from ISO1212 chip. So ISO1212 temperature rise is less.
What is more, If it sets 4V and 3V, I can use it in 5V input system rather than type1/2/3 and replace opto IC. It can cover more application.
Do you think if it makes sense?
Thanks!