Other Parts Discussed in Thread: ISO7721, ISO7720,
Team,
ISO7220/ISO7221 datasheet says:
1) Vih min/max:
page 1 -> The M-option devices have CMOS VCC/2 input thresholds and do not have the input noise filter and the additional propagation delay.
Page 8 -> ISO722xM: Vih 0.7*Vcc
Which one is correct?
2) Voh/Vol:
page 11 -> Can you please confirm that all ISO7720/ISO7721 listed in the datasheet have the same Voh/Vol specification?
Thanks in advance!
A.