Other Parts Discussed in Thread: ISO7741,
Hello E2E,
in the maximum ratings, the output current is limited to +/-15 mA.

Is this value related to a maximum peak output current value or is this an output average / rms value?
In an actual application, the output shall drive an RC Filter with 47R in series to a filter capacitor of 22pF. The output peak with 5 V Supply
is therefore 5V / 47R = 105 mApeak. Is this allowed or does this exceed the absolute maximum rating?
Regards Christian