Hi experts,
My customer selected ACNT-H61L-500E considering the reinforced insulation.
Do we have suitable device to replace ACNT-H61L-500E?
Many thanks!
BR,
Gordon
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Gordon,
Thanks for reaching out.
ACNT-H61L-500E is an opto-isolator with logic output in a 15mm width package. We do not have a pin-compatible device to this but we do have 14.5mm wide DWW 16-pin SOIC package for ISO78xx family that offers higher working voltage than ACNT-H61L-500E. If customer requires more than one channel, then ISO78xx can offer upto 4 channels in a single DWW package with desired channel direction configuration thereby saving significant amount of board space.
Please do share information related to this part with customer and let us know it meets all their requirements. Thanks.
Regards,
Koteshwar Rao
Hi Koteshwar,
Thanks for your comment, I think ISO7821DWWR is suitable considering your recommend.
Thanks!
BR,
Gordon