Hi,
The chip is used as I2C isolation, with MCU 3.3V IO on the input side and CH452 5V on the output side. According to the recommended schematic design, the signal on both sides has 2.2K pull-up, and the power supply is decoupled by 0.1uF.
The specific phenomenon is that after the chip continues to work for a period of time (2-8 days), the high level of SDA and SCL on the output side drops to 2V or 0V, and internal damage is suspected. The fault reoccurs some time after the device is replaced.
The output side is an independent circuit board, the test cable is larger than 6 meters, and the communication rate is 100K.
Please help to check what is the problem? Many thanks~