Other Parts Discussed in Thread: ISO6721, ISO1044, ISO1042
I am referring to the following reference design: Isolated CAN FD Repeater Reference Design (Rev. A) (ti.com). The design supports a 2 Mb CAN data rate. However, the digital isolator used in the design, ISO7721, can support a data rate up to 100 Mb. Is there any particular reason the digital isolator data rate needs to be so much higher than the CAN transceivers data rate? I'm considering using a digital isolator with a lower data rate that's closer to the CAN transceiver, but curious if I'm missing something here that'd cause this to be a bad idea.