This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1640: Compatibility between cc13xx/cc26xx family and ISO1640/ISO1540

Part Number: ISO1640
Other Parts Discussed in Thread: CC1312R, ISO1540,

Hi,

In Section 6.9 in ISO1640 and ISO1540 datasheets I see the low-level output voltage on side 1 (V_OL1) to be max 710 mV and 800 mV respectively for the two devices. Looking at the datasheets for the cc13xx/cc26xx family I see the GPIO voltage input threshold (V_IL) to be 0.2 * VDDS, which at the common voltage of 3.3 V is 0.66 V (see e.g. Section 8.21.6.1 in cc1312r datasheet).

Am I understanding correctly that the ISO1540/ISO1640 is thus not compatible with the cc13xx/cc26xx family at 3.3 V?