What is Maximum Working Isolation Voltage (VIOWM) and Maximum Repetitive Peak Isolation Voltage (VIORM)?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
What is Maximum Working Isolation Voltage (VIOWM) and Maximum Repetitive Peak Isolation Voltage (VIORM)?
Please note that all definitions and references are based on the latest standard IEC 60747-17
VIOWM – Maximum Working Isolation Voltage
VIORM – Maximum Repetitive Peak Isolation Voltage
Definitions:
VIOWM - An RMS or equivalent DC voltage assigned by the manufacturer, characterizing the specified long term withstand capability of its isolation.
VIORM - A peak voltage assigned by the manufacturer characterizing the specified withstand capability of its isolation against repetitive peak voltages. It includes all repetitive transient voltages but excludes all non-repetitive transient voltages.
From which certification/standard are these specifications derived?
DIN EN IEC 60747-17 (VDE 0884-17)
How are they specified in TI datasheets?

How are they validated?
The working isolation and maximum repetitive peak isolation voltages are validated using a partial discharge test, which verifies there is no degradation of the insulation from the absence of localized discharges within the insulation. Since a partial discharge test is included in both Method a and Method b tests, the working isolation and maximum repetitive peak isolation voltage can be validated during qualification and production testing.
End of life testing and accelerated stress testing is also conducted to verify the working and maximum repetitive peak isolation voltages. Accelerated stress testing, often referred to as time dependent dielectric breakdown (TDDB), involves the following:

Why do these specifications matter and how are they relevant to isolated systems?
Certain applications will have high voltage levels applied across the isolation barrier frequently and/or continuously over the course of the product’s lifetime. The maximum working voltage quantifies the maximum RMS or DC voltage that the isolator can safely support over the course of normal operation. The maximum repetitive isolation peak voltage quantifies the maximum periodic voltage the isolator can safely support over the course of normal operation. It is important for the isolation barrier to have a certified working and maximum repetitive peak isolation voltage greater than or equal to the voltage seen across the barrier to ensure that the barrier does not fail within the device’s lifetime.
How is reinforced isolation defined?
For a reinforced isolation rating, accelerated stress testing must prove that the isolator can withstand a voltage of 1.2 x VIOWM for over 30 years.
Other notes:
The main difference between the working isolation voltage and the maximum repetitive peak voltage is the units used to define the specification. The maximum repetitive peak voltage is defined as a peak value, while the working isolation voltage is defined as a RMS voltage value. Under sinusoidal stresses the working isolation will be the same as the maximum repetitive peak isolation voltage.
ISO6441 and ISO6041 are the latest digital isolators that meet most application requirements. For more device options, please refer to the link below where you can filter devices by various parameters.
https://www.ti.com/product-category/isolation/digital-isolators/products.html