This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISOW7741DFMEVM: ISOW7741DFMEVM not sending data as digital UART ISOLATOR

Part Number: ISOW7741DFMEVM
Other Parts Discussed in Thread: ISOW7741, ISOW7721

Hello Team,

I'm evaluating ISOW7741DFMEVM for isolating UART Signals.

My Setup is as follows

CP2102 (USB/UART Converter) TX is connected to INA of the EVM

MCU RX is connected to OUTA of the EVM

MCU TX is connected to INB of the EVM

CP2102 (USB/UART Converter) RX is connected to OUTB of the EVM

 

The Hardware Setup is 

CP2102 - ISOW7741- MCU

The input to ISOW7741 is  3.3V and VISOUT of the integrated DC-DC Converter is also 3.3V which is going to the MCU and other peripherals like ADC etc.

The issue is that with the above Setup , My UART is not working as no data is being transferred to the PC.

If I remove the ISOW7741 from between both the IC's the UART Works fine. 

kindly suggest