Hi We are using this ISO6761DWR one of our product.,
We are using one more programmer device in parallel (either one connect at a time),
Other programmer used from IAR I-JET programmer , This is Always high state in normal.
My query is since the IAR I-JET is high state in normal, at the time accessing the ISO6761DWR line in low state (providing low logic at input) will it consider as Logic Low ? because other one (IAR I-JET) in high logic in normal.
Is ISO6761DWR is totem pole output type ?