Part Number: ISOS141-SEP
In my application, I don't need to use some of the channels of the ISOS141-SEP. For the unused channels, how should I connect the unused I/O pins (left open, pull-low, pull-high, etc)?
thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Part Number: ISOS141-SEP
In my application, I don't need to use some of the channels of the ISOS141-SEP. For the unused channels, how should I connect the unused I/O pins (left open, pull-low, pull-high, etc)?
thanks!
Hello,
Thank you for your question!
For an application, leaving unused pin as floating could cause the device to be less immune to noise. In order to immune to noise, you can set the channel input to its respective default state.
Since the ISO141-SEP (non-F version) has a default output of HIGH, a pull-high would have to be used (connect to VCC) to make the device more immune to noise.
Please refer to this FAQ for more detail: e2e.ti.com/.../faq-can-unused-channel-pins-on-a-digital-isolator-be-left-floating
Regards,
Aaditya Vittal
Hello,
What's the impact of having pull-down (10kOhms) or (0Ohms) to Ground instead of having pull-up resistors for the ISO141-SEP (non-F version) for unused pins? The output is left open.
Does this impact the behavior of the IC ?
Thank you,
Hello,
Thank you for your question!
I have answered your questions below:
Regards,
Aaditya Vittal