HI team,
Could you pls kindly let me know the IQ of the ISOM8710 when there is no input signal and output is low? Will it be uA level?
I have a project requires very low IQ signal isolators.
Thanks
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI team,
Could you pls kindly let me know the IQ of the ISOM8710 when there is no input signal and output is low? Will it be uA level?
I have a project requires very low IQ signal isolators.
Thanks
Hello Cheng,
Based on your description the IQ parameter will match to Icch and IccL in the datasheet. Please see below highlighted section.
Let me know if this answers your question or if it is low enough for your application.
Best,
Andrew
No, it's very high. May I understand why the IQ so high, even when there is no signal transimission?
Hi Cheng,
ISOM8710 was designed to be drop in replace with the industry's most common option-couplers. Currently there is no lower current opto-emulator. We do have a digital isolator designed for low current applications (ISO7021 Ultra-low power consumption – 4.8 μA per channel quiescent current at 3.3 V)
Please let me know if there is a specific opto-coupler solution that you are trying to drop in replace.
Best,
Andrew