Hi, Support Team
We use ISO6721-Q1. INB pin connected to GND, When power on and we find OUTB have peak voltage 2.92V
is normal?
note: OUTB Pin is floating
Schematic:

SCOPE:

if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi, Support Team
We use ISO6721-Q1. INB pin connected to GND, When power on and we find OUTB have peak voltage 2.92V
is normal?
note: OUTB Pin is floating
Schematic:

SCOPE:

if any suggestion, Please advise me.
Thanks,
Best regards,
Lawrence
Hi Lawrence,
Thank you for your question.
It is important to consider the default state of the device. The ISO6721-Q1 has a default state of HIGH. Since the INB pin is pulled to ground, this is driving the INB state LOW, which is not default state. The ISO6721-Q1 device stays at default state when powering up. once fully powered up, the device will pass the input state which is LOW. Please refer to Section 9.4 in the datasheet for more information in regards to the logic states when VCC is powered up or powered down.
Regards,
Aaditya Vittal