This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1212: Whether the IC Will sense both 12V & 24V Dry contact Input Signal?

Part Number: ISO1212

As a one of our project Implementation, we planned to use ISO1212

To sense the dry contact Input signal which are in the range of 12V & 24V.

So, could you please suggest the reference circuit with component details including Rth & Rsense resistor configuration if any

  • Hello,

    Thank you for your question.

    Can you please re-attach the image as I unable to view it?

    The ISO1212 supports a voltage range of 12V to 60V for the SENSEx and INx pins, so the ISO1212 should work for your application as 12V and 24V is within the voltage range.

    Regards,
    Aaditya Vittal