Hello TI
Can you provide me the formula how to calculate Isolator ISOW7741-Q1 power consumption of this Chip?
Output load current at VISO5V0_ISO is 30mA
Regards
Gaurav Mayekar
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello TI
Can you provide me the formula how to calculate Isolator ISOW7741-Q1 power consumption of this Chip?
Output load current at VISO5V0_ISO is 30mA
Regards
Gaurav Mayekar
Hi Gaurav,
Thanks for reaching out.
The power consumption of device under various test conditions is listed in the datasheet. Please allow me to make some assumptions on test conditions for your case and provide an example for estimating current consumption.
Please note that the actual current consumption could be slightly different because the actual test conditions could be different from what are assumed. For example, VDD and VISOOUT voltages are assumed as 5V but might be slightly higher or lower in during the test.
I would also like to mention that datasheet doesn't provide specifications for individual temperature values as that would be impractical. Instead it provides specifications for typical, min and max operating conditions. For calculations, please use worst-case values (min or max depending on parameter) to get worst-case calculations. Thanks.
Regards,
Koteshwar Rao