This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7763-Q1: Finding the number of transistors used in the IC

Part Number: ISO7763-Q1


I am Hardware Safety engineer working on reliability work for powertrain application. I am working on software" Ansys medini" where we can calculate the fit rate of any active and passive component as per our environment. Therefore , I need few information related with the IC "ISO7763FQDWRQ1"

1. What are number of transistor used to manufacturer this IC controller ?
2. What is the material substrate used for packaging of IC in detailed ?