Part Number: ISOW7842
Other Parts Discussed in Thread: LP2985A, , ISOW7742
Hello!
I'm supplying the LDO LP2985A with the output of a ISOW7842 (3.3V primary driven). The output can be as low as 3.13V (for currents up to 30mA) and the dropout voltage of the LDO can be up to 148mV for currents up to 10mA.
So my input voltage to the LDO can be lower then 3V in very worst case conditions at least theoretically. Meaning that the LDO fully turns on. I want to avoid that and guarantee an input voltage higher than 3V at any time.
The ISOW7842 has a very broad input voltage range with 3.3V +-10%. I'm feeding 3.18V minimum to it and am therefore far above the -10% limit.
So my question is, does the input voltage of the ISOW7842 correlate to it's output voltage?
Meaning that when I have at least 3.18V at the input, I must not count with the minimum output voltage of 3.13V?
Thanks and best regards!
Patrick