Other Parts Discussed in Thread: ISO7741
Hello,
I'm using ISO7741-Q1 (non-F version) in an automotive project.
From Table 8-2 Functional Table it is clear that the output will be HIGH, when VCCI is "powered down (< 1.7V)" and VCCO is powered up.
What happens when VCCI is falling and it is between 1.7V and 2.25V?
Can the output be set to HIGH in this undefined region? Or does VCCI really have to fall below 1.7V before the default output mode can trigger?
Thanks!
Utku