This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6760: Maximum allowable input voltage for ISO6760DWR

Part Number: ISO6760


Dear TI team,

I am using ISO6760DWR as digital isolator in my circuit. Input side Vcc is 3.3 V but input PWM signal is 5 V.

Vi is higher than Vcci but it is below absolute maximum rating. Will this configuration damage my circuit or it is okay to use?

Thanks,

Shritesh