This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6740: Need Optocoupler for the specific Industrial appliczations.

Part Number: ISO6740


Hi Good Evening,


Can you suggest the, Optocoupler part number for the below requirements mentioned for the Industrial application.

-Isolation Voltage       >1000V
-Isolation Resistance 10M Ohms @ applied voltage of 1000V
-Degree of Contamination Class II as per IEC 60664-1
-Over Voltage Category Class II as per IEC 60664-1
-Operating Temperature 20 to 60'C

Regards,

Sangeeta