Part Number: ISO7761
Other Parts Discussed in Thread: ISO6761
Hi team,
ISO7761 does not support 1.8V. Is there any similar device that can support 1.8V?
BR,
Comi
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Here is a search for 5+1 isolators: ti.com/isolation/digital-isolators/products.html#1498=Catalog&2877=5 forward / 1 reverse
The ISO6761 supports 1.8 V, but is slower.
Hi Comi,
Thank you for your question.
As Clemens stated, the ISO6761 device supports VCC=1.8V operation, but supports a lower data rate of 50Mbps.
The ISO7761 only supports VCC=3.3V and VCC=5V operation with data rate of 100Mbps.
Regards,
Aaditya Vittal
Thank You Clemens!