Tool/software:
Dear TI team,
Testing the input circuit will damage the ISO6760DWR components. I don't know the cause, so I'm leaving a question.
I am using ISO6760DWR parts in the circuit for insulation. The circuit configuration is as shown in the image below.
The input signal to the ISO6760DWR part is configured as the circuit below. The voltage going into the input signal is 72V.
The power source used in the circuit is configured as shown in the image below. It receives the main power supply of 72V and generates 24V, 5V, and 3.3V using a regulator.
Is there a wrong configuration in the circuit?
Thanks.