Other Parts Discussed in Thread: ISO1228
How to set sinking type or sourcing type in ISO1228?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Sinking type: All the LEDx pins need to be <3V. Hence, LEDx pins are connected to GND via LED with drop up to maximum of 3V.

Sourcing Type: All the LEDx pins need to be >3V. Hence, LEDx pins are connected from AVCC through LEDs.