This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO3088: ISO3088

Part Number: ISO3088
Other Parts Discussed in Thread: ESDS552, LMR16030, TSD05C

Tool/software:

HI Dan kisling

i have a question for you.

As you said adding one more TVS to the line will helps to conduct the High current surge( considering 1KV 42Ohm/ 23A since SM712 has 19A(8/20uA)).is it good to have varistor instead which capable of withstand 23A or more?

also i can see Line to line and line to GND in surge test procedures should we need a varistor across A to B, A to GND and B GND?

in a above picture they saying Earth reference is that Earth or Local GND (GND2 for the case ISO3088)