This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO6762-Q1: ISO6762F Power supply

Part Number: ISO6762-Q1


Tool/software:

Hi,

Please clarify what is the difference between these two cases of power supply mentioned here:

Which current is applicable for which condition. Pls clarify what is the significance of these two test conditions.

Thanks in advance.

  • Hello,

    Thank you for reaching out!

    Please see the image below for a detailed labeling of this section:

    Pls clarify what is the significance of these two test conditions.

    These test conditions are specified for when the isolator has DC signal (one state) applied to it. This means that when the device is in a constant state, the current consumption is as specified.

    Regards,
    Aaditya Vittal