Part Number: ISO1211
Other Parts Discussed in Thread: ISOM8710
Tool/software:
Hi team, can the logic input suit 5V & 24V simultaneously? Thanks!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hello Zoey,
The ISO1211 is designed to meet IEC 61131-2 standard digital input thresholds. The voltage input thresholds can be set using Rthr, however, the lowest valid high VIH is 8.25V. Therefore, the ISO1211 cannot support 0-5V logic.
One solution would be to use ISOM8710 with an appropriately sized resistor to turn on (IF>2mA) for both 5V and 24V inputs.
Best,
Andrew