This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7041: IEC60079-11:2023 cl 7.10.2 Differential leakage current

Part Number: ISO7041


Tool/software:

Hi,

because of the new Edition of the IEC60079-11:2023 there are new requirements to signal isolator which are not optical see cl. 7.10.2 (text below).

If no parameter is noted in the datasheet a test can be done. see cl. 9.9. (see text below)

However, I don't want to do the test.

Are there information in the datasheet which show that parameter or is possible to calculate it with a datasheet parameter as shown below?

I use a 115.2kbit Baud rate = appr. 115.2kHz with a supply current of 3.3V max.3.4V.

Is it possible to use from the ISO7041 (rev. D) datasheet the Cio parameter (Barrier capacitance, input to output) with 1.5pF in chapter 7.6 to calculate
the needed differential leakage current?

Calculation example:
U=3.4V (Umax)
C=Cio = 1.5pF
f= 115.2kHz

Xc = 1/(2 x Pi x f x C) = 921.035kOhm
I=U/Xc = 3.4/921.035kOhm = 3.7µA

I need this information for anactual approval.

Thanks

Best regards
Stefan