This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN6507: UL details

Part Number: SN6507
Other Parts Discussed in Thread: UCC14141-Q1

Tool/software:

Hi,

We are using SN6507 in our design and need UL certificate/IEC certificate in the deign.

Regards,

Mayur

  • Mayur,

    TI provides UL/VDE/CQC and other certificates for IC components that specify a level of safety isolation. SN6507 is not an isolated component so what type of component level standard are you requesting? If the the UL/IEC certificate pertains to an end equipment, this is certified on the customer side.

    Examples of TI component level safety isolation certificates are UCC14141-Q1 product folder here and select "Certificate" from the pull down circled below:

    Steve