Other Parts Discussed in Thread: ADS8900B, SN6501, TIDA-01035, , ADS127L21, ADS125H02, PGA855, UCC25800
Tool/software:
The traditional design used to rely on push-pull drivers.
Analog Devices and TI have used this solution in their EVMs. For example, TIDA-01035 uses the SN6501 to isolate the ADS8900B and AFE. Link to TIDA-01035
I have used the SN6501 in many designs. It works right out of the box, and I have never considered alternative solutions.
However, when I saw the release of the UCC25800-Q1, I began to question whether push-pull is still the best approach.
For example, considerations such as hard vs. soft switching or ZVS/ZCS switching, low inter-winding capacitance, and transformer leakage inductance being treated as a feature rather than a bug.
Now, for the question:
- Can I use the UCC25800-Q1 as the isolated power supply for powering an isolated circuit consisting of the PGA855, ADS127L21, ADS125H02, several multiplexers, operational amplifiers, and an STM32U535, with less than 2W peak power consumption?
Requirements:
- Low-noise power rails after the LDOs.
- The highest possible insulation impedance, without significantly degrading the first requirement.
- Voltage rails: +15V, -15V, and +5V.
Design notes:
- I am considering a resonant tank on the primary side.
- I have an isolated CAN bus link between the isolated and PE sides.- SO I have kind of feedback link
- On the PE side, I have an STM32H7, so I can control the frequency of the LLC using the UCC25800 Rt pin via the STM32 DAC.
- Low and no-load control should not be an issue for the LLC.
I am asking this question because I am unsure if it is worth pursuing an unfamiliar path.
Best regards,
Mirtcho