Part Number: ISO1228
Tool/software:
Hello,
I am using ISO1228 receiver and a SOM KRIA K26 to read inputs external to my board. Inputs are related to proximity sensors and they are active low. Reference voltage for field side is 15V, while POWER LOGIC in the attached schematic is 1.8V. As can be seen from schematic, we are using two ISO1228 components with identical configuration, but U21 is working properly, while we are not able to read input signals from U22 correctly. Is there any mistake in the schematics or anything we can modify?

Thank you in advance for your attention,
Maria Vittoria