Part Number: ISOW7841A-Q1
Other Parts Discussed in Thread: ISOW7841
Tool/software:
For the ISOW784x 3.3V to 5V table below, I see the minimum current the VISO supply can provide an external load is about ~40mA. However, I am hoping to power a transceiver with current draws of: 30 mA minimum, 50mA typical, and 70mA maximum according to its datasheet. Are there typical and maximum current values that the VISO supply can provide? Can this isolator support power the transceiver assuming the current draws listed?