This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7221A: Question about the maximum input signal voltage.

Part Number: ISO7221A


Tool/software:

Hello guys,

One of my customers has the following question about the maximum input signal voltage of ISO7221A.

Could you please give me your reply?

Q.
ISO7221A datasheet say on page 1 that All inputs are 5V tolerant when supplied from a 2.8V or 3.3V supply and all outputs are 4mA CMOS.
But on page 4, it shows that Vi(Voltage at IN, OUT) is -0.5V(Min)~Vcc+0.5V in 5.1 Absolute Maximum Ratings table.

Which is correct? 
Are the device all input 5V tolerant or not?

Your reply would be much appreciated.

Best regards,
Kazuya.