Other Parts Discussed in Thread: TXG4041, , ISO6740, ISO7740, ISO6441
Tool/software:
I need voltage level translation product that also provides 12V of isolation between the A and B sides of the IC. Currently looking at the ISO6540 vs the TXG4041 or 8041.
The desire is to provide some level of insulation between the sides of the IC in case of a power supply overvoltage failure on the other side.
It appears that the two families are essentially the same technology with the ground-level translators having a lesser SiO2 insulation barrier. Is this a fair assessment?
Also does the SiO2 barrier protect one side of the IC from I/O or power overvoltage on the other side?