This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO7761: C2000 F28P650 — MISO signal collapses when routed through ISO7761 isolators; works when bypassed --->AD7490

Part Number: ISO7761
Other Parts Discussed in Thread: SN74LVC1G08, SN74LVC1G125

Tool/software:

Hi Team,

We are facing an issue with the ISO7761 isolator used between the MCU and ADC. Please find the details below:

Platform / Parts

  • MCU: TMS320F28P650 (3.3 V I/O), SPI-B

  • ADC: AD7490, VDRIVE = 3.3 V (DOUT/DIN referenced to 3.3 V)

  • Isolation: Two TI ISO7761 devices on the SPI lines (one for the analog section, one for the discrete/control section).

Problem:

  • With either isolator connected to MISO/POCI (ADC→MCU), the logic-high level attenuates and SPI readback fails.

  • When both isolators are removed from the MISO path (direct ADC→MCU connection), the signal is a clean ~3.3 V and communication is stable.

  • The attenuation is observed on both sides of the barrier:

    • At the ADC DOUT pin when tied into the isolator input.

    • At the MCU POCI pin when driven by the isolator output.
      → This suggests the isolator channel is loading or clamping the line.

Test performed:

  • Initially, I removed U69 and connected MISO directly to the MCU, but the issue persisted.

  • Later I found that the same MISO net was also connected to another isolator (pin 7 / pin 10 to ADC output).

  • After lifting that pin on the PCB, the MISO signal became clean and reached the full 3.3 V, and communication worked properly.

Questions for TI:

  1. For ISO77xx in SPI applications, what is the recommended channel assignment for POCI (peripheral→controller) to avoid loading/clamping?

  2. Is it supported to fan the MISO net into two separate isolator channels?

An image of the connection details is attached for reference.

Kindly review and suggest how we can resolve this issue.

Thanks,
Manikandan V