Other Parts Discussed in Thread: MAX3232E, ISOW7821, ISO7821
For context, it is a medical device. ISOW7742 is part of an isolated serial port (which includes a MAX3232E). Isolation requirement is 3kVac for 60s. We want the port to pass IEC60601-1-2 ed 4 requirements (8kV contact, 15kV through the air).
In a previous design based on ISOW7821 I was advised to place the Y1 capacitor between GNDISO and GND (pins 15 and 2). I made provision for a Y1 capacitor (SMD) capacitor in the schematics, DNP by default unless it is needed for EMC. The PCB is small and circuitry is dense, so I am wondering if I really need the Y1 in the design.
Could you advise if Y1 cap is deemed necessary, and if affirmative, should I place it between GND1 and GND2 (similar to ISO7821 design) or between the floating and non-floating GND planes?
PS: picked "Industrial" application as it is closest to mine.