Other Parts Discussed in Thread: ISO1176T, ISO1176
Hello,
If we’re not using the transformer driver on the ISO1176T, what should we do with the D1 and D2 pins?
Thank you, Keith
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Keith,
If the transformer driver section is not being used then the pins D1 and D2 need to be left open (unconnected).
Alternatively if the transformer driver is not required then ISO1176 (non-T) can be used instead.
Regards,
Anand Reghunathan