Hi team,
My customer met a strange issue when using ISO35 in -40C ambient temperature.
They found when the input common voltage of A/B signal is 1.2~1.4V (Case1), the device won't work correctly. ISO35 output is always constant even input is toggling.
But when the input common voltage becomes 1.75V~2V (Case2), the device could work correctly. Detail test condition is as below.
A |
B |
A-B |
|||||
H |
L |
H |
L |
H |
L |
Status |
|
Case 1 |
2.1V |
0.7V |
1.9V |
0.5V |
1.5V |
-1.2V |
No output |
Case 2 |
2.7V |
1.3V |
2.5V |
1.0V |
1.6V |
-1.2V |
Normal output |
My question is, does our device have a regulation on the receiver common input voltage?
Thank you!