Hi Team,
In Silicon Lab datasheet, e.g. SI86xx, the threshold is defined as VT+ 1.67V(typ) and VT- 1.23V(typ).
Do we have the specifications for ISO7321? These specs are required for input voltage tolerant test.
Thanks.
Zhou
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Team,
In Silicon Lab datasheet, e.g. SI86xx, the threshold is defined as VT+ 1.67V(typ) and VT- 1.23V(typ).
Do we have the specifications for ISO7321? These specs are required for input voltage tolerant test.
Thanks.
Zhou
Hi Zhou,
It is not specified in the ISO7321 datasheet but we can calculate the range from VIH and VIL parameters.
VT+ and VT- would range between 0.8V and 2.0V. There would also be a typical hysteresis of 460mV at 5V supply operation. Calculating using the same would give you the below table.
Minimum | Maximum | |
VT+ | 1.26 | 2.0 |
VT- | 0.8 | 1.54 |
Hope this helps.
Regards,
Anand Reghunathan