Part Number: ISO7721
Other Parts Discussed in Thread: ISO7720
To whom it may concern,
I was looking to use the ISO7721DBQ, but would like to confirm if the part performs level-translation if I was to connect VCC1 to 3.3V and VCC2 to 5V?
It is not clear from the datasheet as reference to different voltages on VCC1 and VCC2 is only made to ISO7720 and not the ISO7721. All references to ISO7721 have VCC1 and VCC2 at the same voltage. Please confirm.
Look forward to your response.
Many Thanks,
Bhav