This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

ISO1176: Skew between four ISO1176

Part Number: ISO1176

Dear Technical Support Team,

How is the max skew between four ISO1176 ?

For example, intersil shows tSK (LIM).


Best Regards,

ttd

  • Hi TTD,

    The part-to-part skew parameter is not part of ISO1176 datasheet specification, hence I do not have a guaranteed value to quote for you. From our theoretical analysis, we expect the typical part-to-part skew of ISO1176 (between any number of samples) to be about 4ns. This is the only information that I could help you with in relation to part-to-part skew. Thanks.


    Regards,
    Koteshwar Rao