Part Number: ISO7342FC
Hi Team,
My customer is getting failures on the ISO7342FCDWR IC.
Pin 14, 13, 12, and 11 are directly connected to an MCU and problematic chips have pin 12 voltage lower that the expected.
It is being used for UART communication.
I attached a good response on a good chip and a bad response on a bad chip.
From the waveforms, the good chip is at 3.3V level while the bad chip is only at 2.5V (channel2)
Channel 1 is pin 13. Channel 3 is pin 11.
Good chip:
Bad Chip:
Here is their schematic:
Here are the tests they have done:
- I noticed that there is no UART response and saw that the pin 12 input has lower amplitude ~2.5V.
- I lifted pin 12 on the Isolator and the signal from the MCU now reaches 3.3V.
- I replaced the Isolator with a new one, and the signals are working perfectly.
- I again, changed the Isolator on the same board with the bad Isolator and took the waveforms I sent to you which is still ~2.5V.
- Then again, changed the Isolator on the same board with the known good Isolator and took the waveforms I sent to you which are at 3.3V.
Do you have any insight why this is happening to our part?
Thanks!
Best Regards,
Alfred